{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Testing your Geo SCADA application after an upgrade
Below are some common areas to test after an upgrade to a newer version of Geo SCADA takes place:
  • The database server starts as expected, no errors occur during the start up
  • The server’s license is being recognized
  • The ViewX clients are licensed and connect to the database server as expected
  • All outstations are able to communicate to their respective devices
  • Data arrive as expected from the outstations
  • Mimic navigation works as expected
  • Mimic scripts are able to run without errors
  • For redundant systems:
    • All redundant servers are able to synchronize with the main server
    • Server changeover works as expected
  • For Virtual ViewX:
    • Virtual ViewX server is upgraded as well as the rest of Geo SCADA
    • Virtual ViewX clients are able to connect to the database server
  • 3rd party clients are able to connect to Geo SCADA and perform their tasks

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: