{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV212 BACnet Unit load and transceiver specifications.
Issue:
What is the BACnet unit load and Transceiver specs for ATV212 Drive?

Product Line:
ATV212, Altivar 212

Environment:
All

Cause:
NA

Resolution:
Below complete data for ATV212 BACnet:

Transceiver Type

- RS485 Transceiver Fail Safe or non-failsafe ? RS485 Transceiver Fail Safe on ATV212.

Transceiver Load

1) What is your unit load ? 32 unit load can be placed on the bus.

2) What is your transceiver load ? 1 unit load.

3) What is your local bias load ? In ATV212 circuit, no bias resistor, but we have a termination of 120 Ohm managed by switch SW103.

ATV212 RS485 description

Schneider Electric Nigeria