{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to configure EIP buscycle with BMED581020 (IEC 61499)
Context: Example BusCycle EIP configuration (IEC 61499) between BMED581020 and BMEP586040.
EIP configuration BMED581020

BMED581020 EIP configuration buscycle

BusCycleTime must be greater than RPI O -> T + RPI T -> O

Example:
BusCycleTime (80ms) >> RPI O -> T (30ms) + RPI T -> O (30ms)

Note: if there are several devices, take the highest RPI O -> T and RPI T -> O.


Product line:
EAE, EIP, Buscycle, Time, BMED581020, IEC 61499
Environment:
Windows, EcoStruxure Automation Expert 22.0

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: