{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to check the SHA256 integrity of a downloaded file or installer

Here is a procedure to check for SHA256 integrity of a downloaded file or installer:
  1. Open Windows PowerShell.  For example, type PowerShell in the Windows start menu command box.
  2. Type Get-FileHash followed by a space.
  3. Drag the downloaded file or installer onto the Windows PowerShell window after the Get-FileHash command and the space.  Alternatively, enter the full path to the file or installer in double quotes after the space.  For example:
Capture1
  1. Press Enter. The output is similar to the following:Capture2
  2. Compare the PowerShell calculated value with the hash value provided.   If the Hash values match the file integrity is ok.
​​​​​

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.