{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
DTM errors in RemoteConnect after installation
After installation, launch RemoteConnect, and a DTM problem happened.
image.png

if RemoteConnect's DTMs are not installed correctly. See information below for missing catalogues.
DTM error

Solution:
  • To update the catalogue, try clicking the update catalogue button.
  • The installation file for RemoteConnect must be located on the local drive C:.
  • Make sure that the installation 2-RemoteConnect-R-2.7.3_Ecostruxure-Control-Expert-V-15.1.zip file is unblocked.
unblocked
  • Verify under the C:\Program Files (x86)\Common Files that the FDT and Schneider Electric Shared are complete.
FDT
SE shared folder

Schneider Electric Nigeria

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: