{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement of Link150 cable adapter?
Issue:
Is there a replacement for the PH68385, Link150 cable adapter?

Product Line:
Ethernet Gateway Link150

Environment:
All

Cause:
PH68385 cannot be ordered separately.

Resolution:
LV434211 is the same hardware as PH68385, so you can order LV434211 as a replacement.

https://www.se.com/ww/en/product/LV434211/modbus-adaptor-cable-compact-masterpact-rj45-to-open-connector-adaptor-190mm-length/



Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: