{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the units when reading LCR or motor current over Ethernet on the ATV340 Drive?

Issue:

LCR address 3204 motor current units or values for the ATV340 Drives.

Product Line:

ATV340 Drives.

Environment:

All

Cause:

Motor amps are reading to high over Ethernet or address 3204 LCr.

Resolution:

The unit of LCR are

From ATV340 0.75kw to ATV340 15kw, the unit is 0.01A.

From ATV340 18.5kw to ATV340 75kw, the unit is 0.1A .

Schneider Electric Nigeria