{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the disk space required for the install of EcoStruxure Machine SCADA Expert v2020 SP2?
Issue
What is the disk space required for the install of EcoStruxure Machine SCADA Expert v2020 SP2?

Product Line
EcoStruxure Machine SCADA Expert

Environment
Configuration software, HMI / Lite SCADA Runtime Software, Windows 10

Resolution
EcoStruxure Machine SCADA Expert v2020 SP2 requires 2.18 GB of hard disk space for installation.
This is the same for both EcoStruxure Machine SCADA Expert running as a configuration software and for running on as a dedicated HMI running Windows. The installation files and size are the same for both.

Schneider Electric Nigeria