{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to Modify RemoteConnect Objects Associated with Logic Variables Online
Typically if a user wants to manipulate variables in a logic program using RemoteConnect, they can manipulate these in an Animation table. When using SCADApack x70 devices this statement is true only for elementary variables or internal DDT type variables. A user cannot manipulate variables that are of the type "T_SPx70_XXX"

See logic example below with an animation table in the Logic Editor. In this example if a user was to try and manipulate the "Start" variable to start the motor, it cannot be accessed via the Animation table. It also cannot be manipulated by right-clicking on the "Start" variable to change the state in the drop-down menu of the ladder section.

animationlogic

The way to manipulate the "T_SPx70_XXX" objects associated with variables is to use the Object Browsers in RemoteConnect. Please see the example Browser in RemoteConnect below.

browser

Further information about Object browsers, T_SPx70 variables and working online with SCADAPack x70 devices can be found in the RemoteConnect help manuals installed with RemoteConnect

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.