{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Modicon M221 - SMS feature: How to use dynamic phone number?

From the SMS Assistant window of EcoStructure Machine Expert - Basic (SMS Configuration), we have the possibility to define a list of phone numbers.

If the application is configured with a functional level of at least Level 6.1, you can declare the strings in a %MW variable and enter this memory variable in the Value field to use dynamic phone numbers.

Here is an example:
SMS Assistant

Phone_number

Schneider Electric Nigeria