{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why do I get the error message " Controller cannot change operating mode at this stage. Verify that its application is appropriate and the Run/Stop switch or input is in the correct position." when I try to start the controller in simulation mode?
Issue:
Error message "Controller cannot change operating mode at this stage. Verify that its application is appropriate and the Run/Stop switch or input is in the correct position. If the controller is in HALTED state, you must initialize it" when starting the controller in simulation mode


Product Line:
M221, EcoStruxure Machine Expert Basic


Resolution:
The error message "Controller cannot change operating mode at this stage. Verify that its application is appropriate and the Run/Stop switch or input is in the correct position. If the controller is in HALTED state, you must initialize it" is cause by having a run/stop input configured in the EcoStruxure Machine Expert Basic program. You must uncheck the run/stop input in order to start/Run the PLC in simulation mode.
image1

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: