{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between NFC and RFID for Evlink Pro AC ?
RFID (Radio frequency identification) systems consist of a reader with an antenna and a transponder. There are three different RFID frequency ranges : low frequencies, high frequencies and upper high frequencies. RFID can be used for long distances (for example in highway tolls)
 
NFC is based on RFID protocols. It operates on the same high frequency as RFID. Because of the short read range limitations, NFC devices have to be in very close proximity and are used for short distances (for example in phones).
 
Therefore, the main difference between NFC and RFID is the distance at which they can be used.
 

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.