{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the levels en DFB encryption available in Control Expert V15.2?

R&D implemented several features to enhance password protection:

1- Starting from CE V15.0, a HF has been released to reinforce encryption with Hardened protection: If this option is selected, then when inserting a password on a DFB, this password will be stored as hash.

2- With CE V15.0 SP1 release, another layer of encyrption has been added : File encryption. This feature when select encrypts the whole application.

This is the most secure mode.

Schneider Electric Nigeria