undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Machine Expert and M controllers: How to check for forced IOs in the application code?
The following function which is generic for all M controllers will return True in case of forced IOs:

Workaround

The system library CmpApp needs to be added to the Library Manager.

NOTE: This function works for Embedded IOs, TM3 IO modules and TM3 Bus Couplers.

Schneider Electric Nigeria