{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How Can I select Gateway/Bridge Device option in IOSCANNING for M580 CPU ?

Issue:

How Can I select Gateway/Bridge Device option in IOSCANNING for M580 CPU ?

Product Line:

M580

Environment:

EcoStruxure Control Expert

Resolution:

User needs to install EcoStruxure Control Expert 15.1 or higher version and choose the CPU version as SV3.20 or higher in hardware configuration .

2.JPG

Select the check box to enable this feature. The communication module doubles the timeout setting by increasing the number of re-transmissions to 6 (instead of the typical setting of 3).

1.JPG

Here is one demo wireshark trace when M580 reset the TCP connection after 6 times TCP retransmissions without receiving the response of ModbusTCP server device after Gateway/Bridge Device option is selected.

3.JPG

Schneider Electric Nigeria

How Can I select Gateway/Bridge Device option in IOSCANNING for M580 CPU ?

Issue:

How Can I select Gateway/Bridge Device option in IOSCANNING for M580 CPU ? 

 

Product Line:

M580

 

Environment:

EcoStruxure Control Expert

 

Resolution:

User needs to install EcoStruxure Control Expert 15.1 or higher version and choose the CPU version as SV3.20 or higher in hardware configuration .

 

2.JPG

Select the check box to enable this feature. The communication module doubles the timeout setting by increasing the number of re-transmissions to 6 (instead of the typical setting of 3). 

1.JPG

Here is one demo wireshark trace when M580 reset the TCP connection after 6 times TCP retransmissions without receiving the response of ModbusTCP server device after Gateway/Bridge Device option is selected. 

3.JPG

 

 

Schneider Electric Nigeria

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: