{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What firmware version of the BMECRA31210 is required for the when using the Profibus module PMEPXM0100 in a remote drop?
Issue:
Minimum firmware version of the BMECRA31210 required when using the Profibus module PMEPXM0100 in a remote drop


Product Line:
PMEPXM0100, EcoStruxure Control Expert


Resolution:
BMECRA31210 version V2.40 is required if the Profibus module is used in a remote drop.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: