{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an Internal Error 10 on the ATS480 soft start?

Issue:

What can cause an Internal Error 10 on the ATS480 soft start?

Product Line:

ATS480

Environment:

INF10 fault

Cause:

n/a

Resolution:

Would suggest to power down the soft start and recheck all the internal connections.

This error is triggered if the external +24vdc supply voltage is higher than 30v, or lower than 19v.

This fault can also occur if the 24v output current is greater than 200ma.

Measure the +24v to com on the soft start.

Check the +24Vdc supply or the current requested by the load connected to the output +24

Recheck the wiring: Previous wiring of ATS48 (+24 and LO+) is at the same location (+24 and 0V) for ATS480.

Do not connect LO+ from ATS48 to 0V of the ATS480.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: