{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
XPSMCMC10804B can the input filter be changed to go lower than 3ms?

In the SoSafe configurable software, I see that the input has a 3ms filter on it.

it cant be disable it can set between 3 and 250 ms not below

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: