{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

MACHA driver, the Authentication configuration window not displayed correctly.

Issue:
In Machine SCADA Expert, the Authentication configuration window is not displayed correctly for the MACHA driver.

Screenshot of Problem


Product Line:
EcoStruxure Machine SCADA Expert 2020 SP2, MACHA driver.

Resolution:
We saw something similar after changing the display fonts scaling to something different than 100%. So please, set the Scale option for the display to 100% in Windows:

Screenshot of Solution

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: