{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the decommissioning process for the Schneider Electric ConneXium Industrial Firewall?
Use the Secure disposal checklist when disposing a ConneXium Industrial Firewall (TCSEFEA23F3F22) to help prevent potential disclosure of data.

Secure disposal checklist
TaskDescriptionCompleted
Record activitiesDocument disposal actions according to your company’s policies and standards to keep a record of activities.

Factory Reset the deviceTo reset the Tofino SA back to its default state as shipped from the factory with configuration and logs erased, you can perform a 'Factory Reset'

Confirm that power is applied to the Tofino SA and it has completed its start-up initialization.

Press, then release the "Save Load Reset" button three times so that the three LEDs are illuminated. On the first press, the " 1/s" indicator will be illuminated; on the second press, the " 2/L" indicator will be illuminated; and on the third press, the "V.24/R" indicator will be illuminated.

After a few seconds, the Tofino SA will start its factory reset sequence. The " 1/s", " 2/L", "V.24/R", "Mode" and "Fault" indicators will flash simultaneously while the factory reset is being performed.

Once the factory reset is complete, the " 1/s", " 2/L", "V.24/R", "Mode" and "Fault" indicators will turn off. This LED pattern confirms that the Tofino SA is passive and passing traffic without filtering. If the Mode LED is ON, repeat steps 1 through 3 above. If the LEDs are different from the above, please
contact technical support.

Decommission and sanitizeFollow decommission and sanitization tasks as described by your organization or contact your Network Administrator.

Perform records tracking sanitization tasks to remove records in related systems. For example: monitoring SNMP servers.

Disposal and reuseAfter usage, this product must be disposed of properly as electronic waste, in accordance with the current disposal regulations of your county, state and country.


For more information on the ConneXium Industrial Firewall, see https://www.se.com/us/en/download/document/NHA1572901/.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.