{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Unity Pro / Control Expert - How to use custom libraries on other computer and other libset version

Issue

My custom library does not show up on another computer using the software or when I use another version of libset for a project

Product Line

Control Expert, all version

Unity Pro, all version

Solution

To share you custom library with others and also on other version of libset, do the following.

First create an installable family in the Types Library Manager window

Exporting library

Select where the files are saved.

Exporting location

These are the files created

Exported files

To install that library you need to use the "Types Library Update tool"

Importing tool

You need to specify the location of the FAMILY.DSC file. This is also where you specify in which libset version you wish to install this custom library. If you need it in multiple libset version you'll have to do process for each version.

Tool settings

It's done, you should now see the new library in your UNity Pro / Control Expert software.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: