{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Vijeo Designer Targets are compatible with the Siemens TIA Ethernet driver?

Issue: The Siemens TIA Ethernet driver is not showing as an option when the target HMI is set to HMIS5T.

Product Line: HMISCU, HMIGTO, HMIGTU, iPC, HMISTO5, HMISTU, HMIS5T, XBTGT

Environment: Vijeo Designer v6.2

Resolution:

The Siemens TIA Ethernet driver is supported by the following HMI families on Vijeo Designer: HMISCU, HMIGTO, HMIGTU and iPC.

The Siemens TIA Ethernet driver is NOT supported by the following HMI families: HMISTO5, HMISTU, XBTGT.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: