{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why my application does not build when I import some DFB from another application (older version of Control Expert) with same DDT structure assigned?
It could be linked to the following reason :
The DDT structure of the new application may not have exactly the same type as the one in the older application (This can occurs with types automatically created by DTMs, due to DTM evolutions)
The DDT structure may contains hidden variables, thus, Control Expert detects that the types are no more identical and the error is raised.

DDT_DFB,Error
To verify you encounter the same issue, please do export the both DDT in .XSY format (the one coming from the new DFB, and the one already created in the application):
Open the exported files with Notepad and verify both variables types and names are identicals.
For instance:
DFB,Hidden variable,DDT

If it’s  not the case, please change the DDT type in the DFB to match the one already created in the application.
Recommended : avoid to use in a DFB, the DDDTs self-generated by the DTMs

Schneider Electric Nigeria