{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a 4000A I-line distribution section available on a QED2 switchboard?

Issue:

Wants to have an I-line distribution section rated same as his 4000A main bus

Product Line:

QED2 switchboard

Environment:

All

Cause:

N/A

Resolution:

No, The maximum I-line interior made is 3000A and it is only available as single row. Double row interiors are 2000A max.

Schneider Electric Nigeria