{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
PowerChute Network Shutdown v5 reports "Could not connect to Host over the network."

Article available in these languages: Japanese

Issue:
PowerChute Network Shutdown v5 reports "Could not connect to Host over the network." when configuring with VMware ESXi 8 host.

Could not connect to Host

Product:
PowerChute Network Shutdown version 5

Environment:
VMware ESXi 7 or 8 host that VMware vCenter Server does not manage. 

Cause:
Security certificate created with the CN= localhost.localdomain
During the installation of ESXi, the installer generates a self-signed certificate for each ESXi host, but the process is performed before the ESXi identity is configured. This means all ESXi hosts have a common name in their self-signed certificate of localhost.localdomain.



Security Certificate
Solution:
1 - Verify that the ESXi host IP address and/or domain name have been entered correctly.
2 - Verify the ESXi host can be pinged from the PowerChute VM or server PowerChute is running on.
3 - Review the security certificate presented by the host. It should contain the host IP address or domain name as the CN.

If the CN = localhost.localdomain, create a new security certificate after adding the correct domain name to the host.


To generate a self-signed certificate

1 - Login to the ESXi host over SSH
            a. Requires ESXi shell and SSH access to be enabled on the host

2 - Back up the existing certificate files

a. mv /etc/vmware/ssl/rui.crt /etc/vmware/ssl/rui.crt.old
b. mv /etc/vmware/ssl/rui.key /etc/vmware/ssl/rui.key.old
3 - Generate a new certificate that contains the FQDN for the CN value.
           a. /sbin/generate-certificates
4 - Restart the hostd service on the host
          a. /etc/init.d/hostd restart

5 - Login to the PowerChute VM
           a. Edit /etc/hosts file and add the IP address and hostname of the ESXi host
Examples: 192.168.0.100 ESXiHost100.homelab.local or 192.168.0.100 ESXi100 if DNS is not configured. 
For help with editing the hosts file, please see How to edit the hosts file on the system PowerChute Network Shutdown has been installed on to.

6 - Reboot the PowerChute VM
           a. The command is init 6

7 - Login to the PowerChute web interface 
           a. Run the setup wizard

 

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.