{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum number of TCP/IP connections for the BMEP586040S
The maximum number of simultaneous TCP/IP connections on the BMEP586040S is the same as on the BMEP586040.  The following table shows the maximum number of connections for the M580 CPU's.

connections

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: