{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to save multiple variable values in Event Logging to a Single CSV File?

Issue:

Want to save data to USB drive on HMIGTO3410 by following the instruction "Save Variable to a Single CSV File, section 13.1.1.5 in the manual"

Product Line:

Vijeo Designer (all versions)

Resolution:

The following video on How to log data using Event Handling in Vijeo Designer, shows how it can be done:

https://www.youtube.com/watch?v=AvucNI5wELE

In it, they indicate to use 2 Text Resources in order to write the data on 2 lines in the file.

But, in Vijeo Designer, it is possible to use only 1 Text Resources and configure 2 (or more) messages:

Text ressource

Then when configuring the Action that will generate the messages, use only 1 Text Resource but use the 2 messages in the actions instead of 2 Text Resources and only 1 message in each.

Actions configuration

This way would be better suited for the management of messages and what they are used for in the project.

Schneider Electric Nigeria