{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do you need a special DTM file to connect Somove to the ATV650F or floor standing Drives?

Issue:

Connecting Somove to the ATV650 floor standing drives.

Product Line:

ATV630F and ATV650F or Floor Standing Version ATV630 or ATV650.

Environment:

All

Cause:

DTM software for Somove to connect to the ATV650 Floor standing drives.

Resolution:

The standard ATV600 DTM will include the option for the ATV630 and ATV650 floor standing drives.

Altivar Process ATV6xx DTM Library DTM files | Schneider Electric (se.com)

Example below:

DTM somove example 1

Schneider Electric Nigeria