{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the LVCT (iEM series) and Power tags have test certificates?
Issue Description:
Do the LVCT (iEM series) and power tags have test certificates?

Product Line:
iEM3455, iEM3465, iEM3555, iEM3565, iEM3455C1, iEM3455C2, A9MEM1520, A9MEM1521 A9MEM1522, A9MEM1540, A9MEM1541, A9MEM1542

Resolution:
  • IEM Meters belongs to the LVCT series and it does not have test certificates.
  • Power Tags: The compliance is achieved by performing 100% product calibration and applying the relevant quality procedures such as ISO 9001 during the manufacturing process. So, for power tag test certificates are not applicable.

Schneider Electric Nigeria