{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you read the ATV630 and ATV930 Drives serial number of Modbus or Ethernet?

Issue:
Reading the ATV630 and ATV930 Drives serial number over Modbus or Ethernet.

Product Line:
ATV630 and ATV930 Drives.

Environment:
All

Cause:
reading Drives serial number over serial communications.

Resolution:

ATV630 with serial number example 4002200HL444562001 you can read this serial number over the serial communications like Modbus or Ethernet.

Read parameters will be C1P1 thru C1PA Address 3410 thru 3419 in HEX than convert the HEX value to ASCII so you have will have 2 bytes per word.

C1P1= logical address 3410  =0X3430 Hex  =40 ASCII
C1P2= logical address 3411  =0X3032 Hex  =02 ASCII
C1P3= logical address 3412  =0X3230 Hex  =20 ASCII
C1P4= logical address 3413  =0X3048 Hex  =0H ASCII
C1P5= logical address 3414  =0X4c34 Hex  =L4 ASCII
C1P6= logical address 3415  =0X3434 Hex  =44 ASCII
C1P7= logical address 3416  =0X3536 Hex  =56 ASCII
C1P8= logical address 3417  =0X3230 Hex  =20 ASCII
C1P9= logical address 3418  =0X3031 Hex  =01 ASCII
C1PA= logical address 3419  =0X0000 Hex  =-- ASCII

Schneider Electric Nigeria