{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Geo SCADA, x70 Controllers and Realflo compatibility

Realflo support for SCADAPack x70 controllers was first introduced in Geo SCADA 2020; offering support for flow computer 7.0

Realflo support for SCADAPack 47x controllers was first introduced in RemoteConnect 2.4.1 offering support for flow computer 7.01

Geo SCADA 2021, Geo SCADA 2022 and Geo SCADA 2023 have support for later versions of Reafllo flow computer and x70 firmware versions.

This document aims to assist users in understanding which versions of Realflo flow computer and SCADAPack x70 firmware are supported by Geo SCADA and RemoteConnect.


Taken from 'What's New' in Geo SCADA Expert 2020 (ViewX Help)

2020 what's new

Taken from 'Driver Reference | SCADAPack Modbus Realflo Driver | Introduction to the SCADAPack Modbus Realflo Driver' (ViewX Help)

2020 Realflo

Taken from 'Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver' (ViewX Help)


2020 firmware

In Geo SCADA 2021, support has been extended for x70 controllers runing flow computers 7.02


Taken from 'What's New' in Geo SCADA Expert 2021 (ViewX Help)

2021 what's new

Taken from Driver Reference | SCADAPack Modus Realflo Driver | Introduction to the SCADAPack Modbus Reaflo Driver (ViewX Help)

2021 Realflo



Taken from Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver (ViewX Help)

2021 firmware

In Geo SCADA 2022, support has been extended for x70 controllers running flow computers 7.10.2


Taken from 'What's New' in Geo SCADA Expert 2022 (ViewX Help)

2022 what's new

Taken from Driver Reference | SCADAPack Modus Realflo Driver | Introduction to the SCADAPack Modbus Realflo Driver (ViewX Help)

2022 Realflo


Taken from Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver (ViewX Help)
2022 firmware

In Geo SCADA 2023, support has been extended for x70 controllers running flow computers 7.11

Geo SCADA 2023, March 2024 Update (and newer) includes support for Realflo flow computer 7.12


Taken from 'What's New' in Geo SCADA Expert 2023 (ViewX Help)
image1a
Taken from Driver Reference | SCADAPack Modus Realflo Driver | Introduction to the SCADAPack Modbus Realflo Driver (ViewX Help)

image2a

Taken from Driver Reference | SCADAPack x70 Driver | Introduction to the SCADAPack x70 Driver (ViewX Help)

image3

Summary of Realflo functionality added to RemoteConnect


RemoteConnect R2.4 added support for SCADAPack470

RemoteConnect R2.4.1 supports Realflo flow computer 7.01 (47x controller only) and contains firmware 9.4.2 (supported by Geo SCADA 2020)

RemoteConnect R2.7.2 supports Realflo flow computer 7.10.1 and contains firmware 9.7.2

RemoteConnect R2.7.4 supports Realflo flow computer 7.11.1 and contains firmware 9.7.4 (supported by Geo SCADA 2021 and Geo SCADA 2022)
RemoteConnect R3.0.2 supports Realflo flow computer 7.12.1 and contains firmware 9.8.5 (supported by Geo SCADA 2023, March 2024 update and newer)



Unlike the Realflo software that will connect to an x70 controller and read out all values from the flow computer, Geo SCADA requires users to create 'Reaflo' analog input points' which map to different flow computer register types (I.E. Input, Flow Calculation, Hourly History, Daily History, etc).

Schneider Electric Nigeria

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: