{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EADM does not reflect PLC in NOCONF state when using EADM V3.1 or coming V3.2 to connect M340/PRA
Description:
  • When an M340 or BMXPRA PLC is in a "NOCONF" state and upon connecting via FTP or USB on EADM: --> the "Mode" section in Device List only shows "NOCONF" for a few seconds and then displays "STOP".
Expected/Normal behavior:
  • On Unity Loader, when M340 or PRA PLCs are NOCONF, the NOCONF state is displayed properly and does not get replaced by STOP after a few seconds.
  • On EADM, when an M580 PLC is NOCONF, the NOCONF state is displayed properly and does not get replaced by STOP after a few seconds.
Note:
  • The same behavior was observed on BMXPRA0100 (FW V3.51IR07) modules and on multiple FW versions of P34 2020:
  • V3.30IR10
  • V3.40IR08
  • V3.50IR08
  • V3.51IR07
This issue is planned to be fixed in EADM V3.3, Q2 2024.

Schneider Electric Nigeria