{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Lexium P Robots version are washdown and non washdown?

Only the IP class of the robot does not reveal whether it is a washable or non-washable version of the Lexium P robot, as our motors already reach IP65.
The washdown version is better/easier to clean; there are no places where water can accumulate, everything is protected by the housing (cables and motors).

Overview washdown and non washdown
Exceptions are:

  • VRKP4L0RWD00000
  • VRKP4L0FWD00000

These two P4 types have ILM motors with closed standard housing, therefore are washdown, too.

See also "Housing type" inside Lexium P Robot Hardware Guide.

Schneider Electric Nigeria