{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to change the position of an automatically generated MC12 sytem in Machine Expert Twin?

Depending on the specific application, you may want to integrate a MC12 system into a larger machine model. To do this, you must first have the MC12 system generated by Machine Expert Twin. During generation, Machine Expert Twin creates a separate section for all MC12 related objects. Afterwards you can integrate the section and all MC12 objects in your model.

In order to be able to move the MC12 system in the model, you can simply select the section and change its position. This will move all MC12 objects together. Moving individual MC12 objects can cause problems and interrupt the track.

All other objects of the machine model should then be organized in separate sections.

Screenshot of MC12 section in Machine Expert Twin

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: