{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to manage vibrations in our Weight PMESWT0100 module?

Recommandations:  if the scale is located in an environnement with vibrations there is a logical filter which can be adjust in the DTM of the PMESWT0100.
DTM configuration screen

  • In most of the cases, we adjust the low-pass cut off frequency on 15hz or 20 hz.
  • The AD converter rate which means number of sampling per second can be adjusted to a value "200".
  • At least we recommand to adjust the Mean-filter setting to 16. This performs a moving average of the weight.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: