{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Downloading RemoteConnect

To download and unzip RemoteConnect follow the instructions below.  At the end of this the RemoteConnect installer should be accessible and the installation instructions ready to follow.

  1. Navigate to https://exchange.se.com/shop
  2. Click Login / Register to set up an account or to log in.
Login/Register Dialog
  1. If needed, set up an account, otherwise, proceed to the next steps.

If this is the first time you are downloading RemoteConnect software,

  1. Search for RemoteConnect.
  2. In the search results, click RemoteConnect for the SCADAPack x70.
  3. Review the details on the Overview page.
  4. Click Download.

If you have downloaded RemoteConnect software previously,

  1. Click Purchases and Downloads and select My Digital Library.
My Digital Library
  1. On the My Digital Library page, for RemoteConnect for the SCADAPack x70, click Download.
Download Installer

Unblocking Zipped Files

Files downloaded from the internet may be blocked by Windows. You may need to unblock the files before unzipping and installing.
To check if files are blocked
  1. Right-click on the file.
  2. Select Properties > General.
  3. Check Unblock.
Blocked Image
  1. Click Apply and then OK.
If the downloaded files are not blocked, the Properties > General tab will look similar to the following:
Unblocked Image

Verifying that .NET is Enabled

Enable Microsoft .NET Framework 3.5.
  1. In the Windows search box, enter Turn Windows features on or off.
Windows Features
  1. In the search results, click Turn Windows features on or off.
  2. Click in the .NET Framework 3.5 (includes .NET 2.0 and 3.0) checkbox to enable this feature.
.Net
  1. Click OK.

Unzipping the Files

  1. In your Downloads folder, select the file and extract the files to your local hard drive.
Do not install from a USB device or a network drive.
  1. Double-click the unzipped folder.
  2. Review and follow the installation manual located in “Software Installation.pdf”
Installation Instructions

The installation instructions document just opened contains the instructions required to continue the installation.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: