{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I start-up/turn on BE900G3 and BE1050G3?

Issue:
How do I start-up/turn on BE900G3 and BE1050G3?

Product Line:
BE900GE and BE1050GE

Environment:
All Serial Numbers


Steps / Procedures:

1. Connect the internal battery (
The Back UPS is shipped with one battery cable disconnected).

Follow the series of steps stated below:

Connect battery first.JPG


2. And when the battery is connected successfully, plug it into the Utility or AC main source.
wall outlet connection
3. Press the POWER button. It will illuminate green, and a single short beep indicates that the Backups is on and helping to provide protection for connected equipment.
turning on


Additional inputs:

* Self-Test only occur upon start up.
* Intentional manual self-test is not applicable for this particular product.
* Battery replacement for Backups BE900G3 is RBC17 and BE1050G3 is APCRBC164.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: