{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I monitor 2 or more External Battery packs Temperature Sensor for SRTG15KVA and SRTG20KVA?

Issue:

Can I monitor 2 or more  External Battery packs Temperature Sensor for SRTG15KVA and SRTG20KVA?

Product Line:

SRTG15KXLI,SRTG20KXLI

Environment:

All models, All Serial Numbers

Answer:

No! only 1 at a time are able to monitor or attached to the UPS.

Some customers may attempt to monitor  2  or more  external battery pack  temperature sensor but the default is not. They can only attached or monitor a single external battery pack temperature sensor.

Actual connection:

See image below:
Battery Temp.JPG

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: