{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to wire a 3-wire or 4-wire sensor equipped with its own external power supply and not that of the BMX SDI 1602 module?
Context
It is possible to wire a sensor using an external power supply to the BMX SDI 1602 module. It just needs to be referenced to the same potential (0V of the SDI card).
If a sensor generates its own pulses :
  • You cannot use the SDI line monitoring function (just do not use VS1/VS2)
  • And it is very likely that the SDI "sees" the pulses if they last more than 6ms (generally they are <1ms, otherwise in this case they must be filtered by the application).

This is if the sensor signals are isolated from the sensor PWS :
 sensor_4_wires
In the other case, as for 3-wire sensors, this could also be :

 sensor_3_wires
Product Line
PLC M580 Safety, BMX SDI 1602

Environment
Microsoft Windows 10, Microsoft Windows Server 2019, Control Expert V15.1, Control Expert V15.2, Control Expert V15.3

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: