{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Maximum Distance Easy UPS 24V UPS Can Be From The Battery Pack
There is no maximum distance for the Easy UPS BVS240XDPDR or BVS480XDPDR to be from the XB005XPDR battery pack. The minimum battery voltage required for start-up is Easy UPS 24V Voltage Requirement

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: