{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why is the boot up time longer on the ATS480, than the ATS48?

Issue:

Customer has a ATS480 and when it is powered up it shows “Welcome to Schneider” boot up screen. They state it takes about 8 seconds for the Soft start to boot up and

it’s unacceptable for their process. Any way to reduce the start-up process?

Product Line:

ATS480

Environment:

Boot up time

Cause:

n/a

Resolution:

The ATS480 have a software and hardware control that is different compared to ATS48.

After a power on of Control voltage (CL1-CL2), the starter needs about 6.5 secs for the wake up.

The reason the boot time is higher on ATS480:

The flash memory is larger and there is a increase in the time of the initialization of the file system.

ATS480 embeds a secure boot and the firmware integrity check time is significant.

Unfortunately, there is not a way to reduce this time.

Schneider Electric Nigeria