{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the correct part number of the SYMMETRA LX Tower Frame Caster (Front and Rear)?
Issue: What is the correct part number of the SYMMETRA LX Tower Frame Caster (Front and Rear)?

Product Line:
ALL SYMMETRA LX TOWER TYPE FRAME  (Power and XBP)

Environment:
All Serial Numbers

Cause:
In unexpected circumstances there are events where sometimes there are modifications or moving of such set-ups to another location which results in a lot of movement of the frame and possibly damage to the caster. And to know the correct part number of the particular caster it is good to know each position and its corresponding part number and description.
Answer:

Symmetra LX does have 4 pcs. of caster:

See the following images below for full details:

Caster 1.JPG

Complete image description of the following casters. (see below)
correct description.JPG
See provided link below for your references:

SYAFSU7 = https://www.apc.com/us/en/product/SYAFSU7/apc-symmetra-lx-castor-kit-    right-front-left-rear/

SYAFSU6 = https://www.apc.com/us/en/product/SYAFSU6/apc-symmetra-lx-castor-kit-left-front-right-rear

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: