Search FAQs
Smart-UPS Ultra 5kW Reports "Battery Modules Not Connected" or "Internal RBM Disconnected" Alarm
Issue: The UPS reports "Internal RBM Disconnected" or "Battery Modules Not Connected" alarm on the LCD.
Product Line: SRTL5KRM2UI, SRTL5KRM2UT
Environment: UPS firmware version 03.1 or earlier
Resolution: This issue is addressed in UPS firmware version 03.2 Upgrade the UPS firmware to version 03.2 or later. Refer to FA170679 or FAQ000242942 for more information on how to update the UPS firmware.
Product Line: SRTL5KRM2UI, SRTL5KRM2UT
Environment: UPS firmware version 03.1 or earlier
Resolution: This issue is addressed in UPS firmware version 03.2 Upgrade the UPS firmware to version 03.2 or later. Refer to FA170679 or FAQ000242942 for more information on how to update the UPS firmware.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: