{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
PowerChute Network Shutdown ESXi host shutdown failed for vSAN standard cluster with Skip Maintenance mode enabled.
Issue:
ESXi host PowerChute Network Shutdown is running on failure to shutdown when configured for vSAN, and enabling Skip Maintenance mode has been selected.

Product:
PowerChute Network Shutdown version 5.x

Environment:
PowerChute deployed onto a vSAN datastore.
VMWare ESXi 7.x or 8.x

Cause:
The PowerChute shutdown delay is set to high.

Solution:
Edit the pcnsconfig.ini file and change the shutdown command duration to 0 (zero) seconds.

Default configuration
[Shutdown]
shutdownCommand =
shutdownCommandDuration = 60

After the change
[Shutdown]
shutdownCommand =
shutdownCommandDuration = 0

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: