{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the maximum number of connections the BMENUA0100 module can open to the M580 CPU?
Issue:
Maximum number of connections the BMENUA0100 module can open to the M580 CPU


Product Line:
BMENUA0100


Resolution:
The number of connections the BMENUA0100 module can open to the M580 CPU depends on the capacity of the CPU. Thus, performance of the BMENUA0100 module will depend on the time required to perform the MAST task and the selected CPU. The maximum number of connections opened by each BMENUA0100 module to the M580 CPU are as follows:

image1

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: