{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to read and modify variable by sending SMS to the Zelio Smart Module?
  1. In ZelioSoft:
When configuring the COM function block, select Variable modification as message Type:
Variable_modification

Regarding the Parameters, select people who are authorized to send Modification command and define the variable access to “Read and modification”:

Parameters
  1. Connection to the Zelio Smart module:
When connecting to the Zelio Smart module through the SR2COM01 the following popup window appears:
Write_options

From this window, define the access key which will be used in the command to read/modify variable(s). By default, it is 00000000.
  1. On Mobile phone:
To read the value of the variable which has the Alias B003, send the following command via SMS: 00000000!B003?

SMS1

To modify the value of the variable which has the Alias B003, send the following command via SMS: 00000000!B003=1
(In that case, the value '1' will be written in the variable having the Alias B003)

SMS2

If the variable and/or the recipient only have the read access, the following error should appear when trying to modify the value:

SMS3

Schneider Electric Nigeria

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: