{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the MotorLogic solid state overload relays be used on Open Delta or Grounded B-phase systems?

Issue:
Can 9065 Solid state overload relays be used in applications with Open Delta or Grounded B-phase systems?

Product Line:
NEMA Contactors and Overload relays


Environment:
9065 Motor Logic Solid-State Overload Relays


Cause:
The overload is tripping when used on Open Delta or Grounded B-phase systems


Resolution:
Open Delta systems or grounded B-phase systems are difficult to balance and could cause the Motor Logic SSOLR to trip. For these systems, it is better to use a Melting Alloy Overload Relay.

Schneider Electric Nigeria