{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to Perform a Logic Reset or "Brain Dead" on a Smart-UPS Ultra 5-10kW?

Issue:
This document explains how to perform the Brain Dead procedure on a Smart-UPS Ultra 5-10kW

Product Line:
Smart-UPS Ultra 5-10kW models: SRTL5KRM2UI, SRTL5KRM2UT, SRTL8KRM4UI, SRTL8KRM4UT, SRTL10KRM4UI, SRTL10KRM4UT

Cause:
The Brain Dead procedure performs a reset of the UPS microprocessor. This is useful for basic troubleshooting to attempt to clear any alarms. It does not however reset saved preferences.

Resolution:
  1. Turn off any connected load.
  2. Turn off the UPS using the LCD Display, and disconnect the AC input.
    • For hardwired units, refer to the User Manual - Deenergizing safety.
  3. Turn off the internal battery module using the Battery On/Off switch.
    • Turn off the battery modules using Battery On/Off switch in any external battery packs connected to the UPS.
  4. Reconnect the internal and any external batteries, reconnect AC input, and turn the UPS on using the LCD Display.
Note: Refer to the UPS Operation Manual for how to turn the UPS and the batteries on or off.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: