{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the transfer time of APC Smart-UPS and Symmetra Units?
Issue:

What is the transfer time of APC Smart-UPS and Symmetra Units?

Product Line:

Smart-UPS and Symmetra Units

Answer:

Transfer time refers to the duration in time it takes the UPS to switch from one state (i.e. Onbattery, Online...) to another.

The transfer time of Line interactive units (SMC, SCL, SMX, SMT and SMTL): High = 2-4ms, Med = 6-8ms, Low = 8-10ms
Note: Lowering the sensitivity will increase the transfer time.
For detailed discussion about power quality and sensitivity is further discussed in FA372508 .

With Double Online Conversion units (SRT, SRTL, SRYL, SURT and SURTD) there is no transfer time.
In the double conversion on line design, failure of the input AC does not cause activation of the transfer switch, because the input AC is charging the backup battery source which provides power to the output inverter. Therefore, during an input AC power failure, on line operation results in no transfer time.

If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.