{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to change the temperature scale of an APC Network Management Card

Issue:
How to change the temperature scale of an APC Network Management Card

Product Line:
AP9619, AP9618, AP9631, AP9635, AP9635CH, AP9641, AP9643

Environment:
APC Network Management Card with environmental monitoring.

Resolution:
A customer may want to change their set temperature scare from Celsius to Fahrenheit and vice versa. This can be dependent on different factors such as policies or standards, ease of use, or just basic preference.

APC by Schneider Electric values this and takes in mind on our Network Management Cards.

You can change the temperature scale of an NMC depending on the firmware revision and/or the NMC model :

On NMC Generation 1 (AP9619, AP9618) or NMC Generation 2 (AP9631, AP9635, AP9635CH) with firmware 5.X.X, you can change this by clicking at Administration, then General, and then Preferences.

Temperature Scale Change on an NMC 1 or old NMC 2 with FW at 5.x.x


On NMC Generation 2 (AP9631, AP9635, AP9635CH) with firmware 6.X.X and above and NMC Generation 3 (AP9641, AP9643), you can change this by either selecting a LOCAL user and configuring it individually or this can be set proactively at the default user configuration settings.

Temperature Scale Change on an NMC2 or 3


If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: